Contato responsável
igus® do Brasil Ltda

Rua Antônio Christi, Nº 611

Parque Industrial III - FAZGRAN

13213-183 – Jundiaí-SP

+55 11 3531 4487
+55 11 3531 4488

Sliding roof drive system

 
manus® 2005

"The bearing tolerances could be clearly enhanced by the machining of the inner diameter of the iglidur® P polymer plain bearing. Enhanced suitability for continuous operation through improved wear behavior compared to the unmachined inner diameter of the plastic bearing. This can be accounted for by the better bearing quality of the inner diameter through the machining. The better guidance of the drive shaft leads to a low wear even during the application. ”

Roland Pretscher, Siemens VDO Automotive AG, Würzburg

More on applied products here
Further interesting applications from extremely diverse areas can be found here.
Go to manus® contest