The carbon profile rails is especially light and strong The carbon profile rail WSPC is 70% lighter than liner rails made of aluminium or stainless steel. Especially in aircraft construction or the automotive industry the drylin® W carbon rail with square profile is used. The solid plastic carriage WWPL-06-30-06 made of an iglidur® material was developed specifically for the carbon rail and has best coefficient of friction and wear. The X-ray transparency is another advantage of the carbon fibre. So the material is often used in medical or measurement technology.
Não tem certeza de que encaixa?
Consultoria
Terei muito prazer em esclarecer suas dúvidas pessoalmente