Você tem alguma pergunta? Precisa de material? Estão disponíveis para download aqui informações de imprensa e material fotográfico pronto para publicação. Ficaríamos também felizes com a sua ligação, e-mail ou fax! |
|
Contato de imprensaGostaria de ser adicionado(a) à nossa lista de distribuição de mídia? |
Harnessing the secrets of nature: the E4Q energy chain from igus wins the German Design Award23/10/2020
After winning a large number of awards in recent years, igus once again proves how progressive design can bring the user concrete benefits. This also applies to the E4Q energy chain. It is striking that igus has taken a new path here. "In order to optimise the material and thus the weight of the energy chain, our developers have been inspired by nature", explains Michael Blaß, head of the e-chain systems division at igus. "The rounded design is very organic and is found on the outside of the chain links and the stop-dogs. This reduces the weight by 10 per cent compared to the previous E4.1 series, and also the drive energy." Despite the material cut-outs, the new development has 20 per cent higher strength and stability. The chain links of this energy chain generation continue to have a completely new crossbar concept with locking straps. These ensure that the series can be opened and closed in seconds without tools. Filling is therefore particularly easy, and the installation time is reduced by 40 per cent.
|