Construction machine

An actuation shaft for thrust bearing of a coupling required new bearings. The existing bronze bushes shrunk over the years and had to be replaced along with the shaft. It was also required to avoid the lubrication points of the axis in future. The result is: iglidur® M250 plain bearings are now applied after about 30 years of exclusive usage of bronze bearings. They are dirt-resistant, lubrication-free and can be easily installed.
Construction machine_01
Construction machine_02

Robert Kretschmer, Auerbach, Germany

Here, you can find the products used

Here you can find further interesting applications from very different areas of use:

Go to manus® competition