7 plain bearings from igus prove mold resistant12/11/2019

Mold is a serious health hazard, and can grow on almost any substance when moisture is present. Air conditioning systems in buildings, aircraft and cars, or anywhere condensation can form or water leaks occur, are areas prone to mold growth.

Plastics can be used by microorganisms as a source of food and by the metabolic products of the bacteria. In a laboratory test, the iglide materials were tested for the appearance of microorganisms using the DIN EN ISA 846 method A. This test examined the resistance of the materials to fungi and bacteria.

For the test, the plain bearings were stored in a special culture for four weeks at 29°C. The result: an alteration was not found on the tested materials (iglide G, G1, J, H1, X, GV0 and J350). There was also no mildew.

In building ventilators and air damper regulators, igus plain bearings offer corrosion resistance and are insensitive to dirt. They are also easy to clean and resistant to temperature, media and chemicals. On aircraft, mold-resistant iglide plain bearings are also used in seat and arm adjustment mechanisms, kitchen storage equipment and luggage lockers.

For more information, visit the igus website.