Oil test with e-chains®

igus® e-chains® are exposed to various materials in various applications. Ranging from metal chips to wood dust and fluids: we have the right solution for your energy supply system, such as RX tubes, AX chains and many others. We subjected our e-chains® to various oils and lubricants in a test. Lubricants are used by many industries for production. It is therefore possible that our e-chains® can come into contact with these lubricants and cutting oils. We have now tested the worst-case and operated our255.10.075.0 e-chain® immersed in various oils for a period of four months Following this time, we compared it with an e-chain® that was not exposed to these substances.
Test setup in the igus® lab Test setup in the igus® lab

Result

On average, the e-chains® under test only lost 10% of their strength. This should be taken into account for planning purposes, and a slightly higher strength e-chain® should be used if it comes into contact with oils and lubricants.

Additional information

Test laboratory for energy chains

More than three billion test cycles per year are carried out at a total of 180 testing stations.